The output terminals of the N6900 and N7900 Advanced Power System are buss bars with holes. Bolts are included to bolt to the load wiring. Ring lugs are usable as long as they can carry the maximum current of the unit.
Refer to the user's manual at http://literature.cdn.keysight.com/litweb/pdf/N7900-90901.pdf for details.
Applies to: N6950A, N6951A, N6952A, N6953A, N6954A, N6970A, N6971A, N6972A, N6973A, N6974A, N6976A, N6977A
Applies to: N7950A, N7951A, N7952A, N7953A, N7954A, N7970A, N7971A, N7972A, N7973A, N7974A, N7976A, N7977A
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |